Device Definition - Configure Relay dialog box parameters

The
Device Definition - Configure Relay dialog box
includes these parameters.
Parameters
Parameter
Description
Slot
Use this menu to configure the slot number for each relay. Valid ranges are 1-6.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal