Time Sync view
How do I open the Time Sync view?
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectTime Sync.
Use
Time Sync
view to view time synchronization status and enable or disable time synchronization on the controller. Enabling time synchronization allows the controller to participate as a clock in the system time. It also allows the controller to become a master clock for the system, or become a master clock in the chassis.If the controller is the grandmaster clock, all devices connected to the controller synchronize with the clock of the controller.
Time Sync
view displays details for the device that is acting as the grandmaster clock.Provide Feedback