View event properties

Use the
Events
view to view event properties for the input devices.
To view event properties
  1. On the tab for the device, select
    Events
    .
  2. In the
    Events
    view, view the parameters for the events.
TIP:
To configure event properties, navigate to the
Tag
editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal