Configure the Cold Junction Compensation for thermocouples
Configure the cold junction compensation when a channel is configured for thermocouple operation.
The channel must account for the thermoelectric effect of a junction of the thermocouple field wires and the RTB terminals.
To configure the cold junction compensation for thermocouples
- On the tab for the device, selectCJ Channels.
- In theCJ Channelsview, configure the settings as needed.
- SelectOKto confirm and save the changes.
Provide Feedback