Event Output Tags
Name | Data Type | Definition | Valid Values |
|---|---|---|---|
Eventxx.En | BOOL | When set, the corresponding event trigger definition is active and events are
triggered when conditions match the definition. |
|
Eventxx.EventRisingEn | BOOL | Triggers an event each time a condition change results in conditions that match
the event trigger definition. | When EO.Eventxx.IndependentConditionTriggerEn = 0 Trigger event (EventRisingEn, EventFallingEn):
When EO.Eventxx.IndependentConditionTriggerEn = 1 Trigger event (EventRisingEn, EventFallingEn):
|
Eventxx.EventFallingEn | BOOL | ||
Eventxx.LatchEn | BOOL | When set, events are latched until acknowledged. A new event is lost if the previous event has not been acknowledged. When not set, new events overwrite old events. |
|
Eventxx.ResetEvent | BOOL | A transition from 0 to 1 resets all events and clears the event queue on the
channel. | 0 or 1 |
Eventxx.IndependentConditionTriggerEn | BOOL | Determines whether an input state change or a pattern of input state changes
triggers an event. |
|
Eventxx.EventNumberAck | DINT | The controller writes back EI.Eventxx.EventNumber into EO.Eventxx.EventNumberAck
to indicate receipt of the event. | All values |
Eventxx.PtxxDataSelect Eventxx.CounterxxSelect | BOOL | Determines whether the channel participates in the event trigger. |
|
Eventxx.PtxxDataValue Eventxx.CounterxxValue | BOOL | Determines the state of the channel that triggers the event. |
|
Provide Feedback