Change device type or revision

Use the
Change type
dialog to change the device type or revision.
  1. On the tab for the device, select
    Overview
    .
  2. In the
    Overview
    view, select
    Device definition
    .
  3. In
    Device definition
    , select
    Change type
    .
  4. In
    Change type
    , in the
    To
    section, specify the device type and revision as needed.
    TIP:
    Changing device type will change, delete, and/or invalidate the device properties that are not valid for the new device type.
  5. Select
    OK
    to finalize the changes and exit the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal