Unlatch service failed

A problem occurred when the device tried to unlatch a process alarm. This problem occurs if the process alarm condition is not configured to latch when an alarm is triggered. To resolve the problem, go to the
Alarms
view, and then select the
Latch Process Alarms
checkbox.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal