Incorrect device
There is a mismatch between the target device and an Analog Output or Input Group object. This error occurs when the device in the software I/O configuration and the actual physical device do not match or the device is configured incorrectly. The mismatch problem must be fixed before attempting the calibration process. Verify that the device is correctly configured, and then update the software I/O configuration to match the device.
Provide Feedback