Scaling to engineering units in input devices

Channel data values in the input tag may be in engineering units such as Bar, Degrees Celsius, Kg/minute or percentage. To configure the relationship between the physical signal in volts or mA and engineering units, set the
Low
and
High Signal
and the
Low
and
High Engineering
values.
For example, a temperature transmitter on channel 3 which produces 4 mA current at -180 degrees C and 20 mA of current at 750 degrees C, and you are using Degrees C in your control program, configure the values as in this table.
Setting
Signal
Engineering
High
20
750
Low
4
-180
If you are using HART field devices, we recommend setting
High Engineering
and
Low Engineering
to the field device’s
Upper Range Value
and
Lower Range Value
so that the field device uses the same engineering units as the 1756-IF8H. If online, these values display in
HART Device Information
view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal