ChX view parameters (input devices)
The
ChX
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
---|---|
Input Type | Displays the input type of the device. |
Input Range | Indicates the operating range and signal type. Valid options are:
Tip : To use HART field devices, select 4 mA to 20 mA . |
Enable HART | Indicates HART communication is enabled on the channel. Enable HART for any channel that has a HART device connected to it to display information in the HART Device Information view.Clear the checkbox to disable HART communication. When HART communication is disabled:
Enable HART is not configurable when:
|
Sensor Offset | Enter the offset value in engineering units, which is added to the channel data after scaling the analog signal to engineering units. Valid values are from -10,000,000 through 100,000,000. The default value is 0.0000. |
Scaling | Defines how the signal from the device corresponds to the measurement data. |
| Defines the unit of the Engineering values. |
| Defines the maximum signal produced by the channel. This value must be greater than the Low Signal value. Default is 20.0000. |
| Defines the lowest signal produced by the channel. This value must be less than the High Signal value. Default is 4.0000. |
| Defines the engineering units that corresponds with a signal value equal to the High Signal .For example, if a temperature transmitter produces 20 mA current at 750 °C, the High Engineering value is 750.This value cannot be equal to the Low Engineering value. Valid values are from -10000000 through 100000000 (float). Default is 100.0000. It is recommended to set the High Engineering value to correspond to the device Upper Range value so that the device and module use the same engineering units. When online, this value is displayed in the HART Device Information view. |
| Defines the engineering units that corresponds with the signal value equal to the Low Signal .For example, if a temperature transmitter produces 4 mA current at -180 °C, the Low Engineering value is -180.This value cannot equal the High Engineering value. Valid values are from -10000000 through 100000000 (float). Default is 0.0000. The recommendation is to set the Low Engineering value to the device Lower Range Value so that the device and device use the same engineering units. When online, this value is displayed in the HART Device Information view. |
Digital Filter | Specifies a filter time constant value from 0 through 20100 milliseconds. The default is 0. This is a first order lag filter that smooths input transitions. (It is called a digital filter because it is done in the software by the device, not by a hardware filter). A value of 0 turns the Digital Filter off. Measured changes in the signal value pass immediately to the controller. |
Provide Feedback