Channels view (output devices)

Use the
Channels
view to:
  • Select the output range and current or voltage mode
  • Enable HART communications
  • Define the output state during Program mode and Fault mode
  • Scale the signal to engineering units
  • Configure HART pass-through
  • Configure the time to keep HART replies
  • Specifies the behavior of the outputs if communications fail in Program mode
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal