Calibration Wizard - Results
The Results view displays the value and status of the enabled channels after calibrating a low or high reference signal.
If the reference signal is within the acceptable range, the status shows
OK
for that channel. Select Next
to continue the calibration process.If the reference signal is not within the acceptable range, the status shows
Error
for that channel. Perform one of these operations:- Correct the signal and selectRetry. After entering a correct value,OKshows in theStatuscolumn.
- SelectCanceland exit theCalibration Wizard, leaving the calibration status for that channel with an Error.
The
Results
view includes these parameters:Parameter | Description |
---|---|
Channel | Allows configuration of the parameters for the channel. The unavailable channels appear dimmed in the wizard. |
Calibrate | Indicates the selected channels to calibrate. |
Calibration Range | Indicates the value currently configured for the channel. |
Low Reference | Indicates the low reference signal that is expected at the input. Only available when calibrating for a low reference. |
High Reference | Indicates the high reference signal that is expected at the input. Only available when calibrating for a high reference. |
Recorded Reference | Indicates value in volts or mA. |
Status | Indicates the status of each channel after calibrating for a low or high reference.
If Status shows Error , perform the corresponding actions as needed:
|
Retry | Restarts the calibration process. |
Provide Feedback