Calibration Wizard - Output Reference

The
Output
Reference
view shows channels to calibrate for a low or high reference and the range of the calibration. Select
Next
to begin producing the reference signal on the selected channels.
The
Output
Reference
view includes these parameters:
Parameter
Description
Channel
Allows configuration of the parameters for the channel. The unavailable channels appear dimmed in the wizard.
Calibrate
Indicates the selected channels to calibrate.
Calibration Range
Indicates the low or high reference signal value that the device produces based on the channel configuration.
Low Reference
Indicates the low reference signal value that the device produces.
Only available when calibrating a low reference signal.
High Reference
Indicates the high reference signal that is expected at the input.
Only available when calibrating a high reference signal.
Back
Returns to the previous page.
Next
Starts producing the reference signal on the selected channels.
Cancel
Cancels the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal