Calibration Wizard - Calibration Complete

After completing the calibration, the
Calibration Complete
view in
Calibration Wizard
shows the status of the calibration for the affected channels. Select
Finish
to close the wizard.
On the tab for the device, the
Calibration
view shows the changes in
Calibration Gain
and
Calibration Offset
. The
Calibration Status
and date of the latest calibration are also updated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal