Calibration Wizard - Attach Reference

The
Attach Reference
view shows channels to calibrate for a low reference or high reference and the range of the calibration at input.
Attach a low calibration reference signal or a high calibration reference signal to the channels to calibrate, and then select
Next
to
produce reference signals on the selected channels.
The
Attach Reference
view includes these parameters:
Parameter
Description
Channel
Allows configuration of the parameters for the channel. The unavailable channels appear dimmed in the wizard.
Calibrate
Indicates the selected channels to calibrate.
Calibration Range
Indicates the value currently configured for the channel.
Low Reference
Indicates the low reference signal value to apply to the channel.
Only available in the
Calibration Wizard -
Attach Low Reference
view.
High Reference
Indicates the value of the high reference source based on the channel configuration.
Only available in the
Calibration Wizard -
Attach High Reference
view.
Back
Returns to the previous page.
Next
Continues the calibration process.
Cancel
Cancels the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal