Calibration view parameters
The
Calibration
view includes these parameters:Parameter | Description |
---|---|
Channel | Displays the number of the channel to which the configuration applies. |
Calibration Range | Indicates the calibration range, as defined in the ChX view by the Input Range or Output Range selections.Valid values are 0 mA to 20 mA for current input and output channels and -10 V to 10 V for voltage input and output channels. |
Calibration Gain | Indicates the calibration gain that is reported by the device. |
Calibration Offset | Indicates the calibration offset that is reported by the device. |
Calibration Status | Indicates the status of the calibration per device. Valid value is OK or Error . |
Start Calibration | Opens Calibration Wizard and starts the calibration process. |
Last Calibration Date | Indicates the date when the device is last successfully calibrated. |
Provide Feedback