SD Card view parameters
Use the
SD Card
view to enable the SD Card to copy configuration files to and from the SD Card. These parameters are not available when offline or a communication error occurs in the device.For duplex devices, you can view the configurations for Module A and Module B. The displayed values become blank in these conditions:
- There is a device type mismatch.
- A timeout occurs while getting the identity from a device.
Parameter | Description |
|---|---|
SD Card status | Displays the status of the SD card. Available values are:
|
SD Card locked | Displays if the SD Card is locked. Available values are:
|
Enable SD Cards | Select to enable the SD Card Slot. Enable SD Cards is disabled when the device is in explicit protection mode. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Writes pending edit to the device. |
Provide Feedback