Port Diagnostics parameters
Port Diagnostics
includes these parameters.Parameter | Description |
|---|---|
Interface Counters | Values only appear when the device is online.
|
Media Counters | Values only appear when the device is online.
|
Reset Counters | Sets the interface and media counter values on the device to zero and updates the values displayed in the dialog box with the current counter values. Reset Counters is only enabled when the device is online. |
Provide Feedback