Overview view parameters (scanner mode)
The
Overview
view includes these parameters when the device is in scanner mode:Parameter | Description |
|---|---|
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Rack connection | Displays the connection to communicate with the I/O devices in the remote chassis.
|
Time sync and motion connection | Displays the Time Sync connection for devices that support Precision Time Protocol (PTP) synchronization.
|
Concurrent communication | Valid values include:
|
Redundant | Indicates whether the device supports controller redundancy. Valid values include:
|
Status connection | Displays the status connect for the device. Valid values include:
|
Network mode | Valid values include:
|
Ethernet Address Module 1 Ethernet Address Module 2 | Specifies the ethernet address for Module 1 or Module 2. These two parameters are only available when the criteria are met:
|
Device definition | Opens Device definition to change the revision, electronic keying, and other device specific values. |
Provide Feedback