Overview view parameters (adapter mode)
The
Overview
view includes these parameters when the device is in adapter mode:
TIP:
The parameters are based on the device being configured. The parameters that do not apply to the device are hidden.
Parameter | Description |
|---|---|
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Rack connection | Displays the connection to communicate with the I/O devices in the remote chassis.
|
Time sync and motion connection | Displays the Time Sync connection for devices that support Precision Time Protocol (PTP) synchronization.
|
Concurrent communication | Valid value includes:
|
Redundant | Indicates whether the device supports Adapter redundancy. Valid values include:
|
Status connection | Displays the status connect for the device. Valid values include:
|
Network mode | Valid values include:
|
Chassis size | Displays the chassis size of the rack that contains the bridge device. Valid range is from 1 through 32. The default is 17. |
Device definition | Opens Device definition to change the revision, electronic keying, and other device specific values. |
Provide Feedback