Internet Protocol - Module view parameters
The
Internet Protocol - Module
view includes these parameters:Parameter | Description |
|---|---|
Internet Protocol (IP) Settings | Specifies the IP settings configuration mode:
|
Physical device IP address | Specifies the address used by the IP protocol to route information to and from the device. |
Subnet mask | Specifies an extension of the IP address scheme that lets a site use a single net Id for multiple physical networks. |
Gateway address | Specifies the gateway device address used to connect individual physical networks into a system of networks. |
Primary DNS server address | Specifies the IP address for the primary DNS server that holds the master copy of the data. |
Secondary DNS server address | Specifies the IP address for the secondary DNS server that holds a copy of the data in case the primary DNS is unavailable. |
Domain name | Specifies the name that identifies the domain in which the device resides |
Host name | Specifies the unique identification string for the device. |
Refresh | Retrieves and displays the latest information from the device. |
Set | Writes pending edits to the device. |
Copy from Module A | Populates the IP Settings Configuration from Module A on the basis of the connection type and the IP settings configuration mode of Module B. Copy from Module A is only available while in Scanner mode and Manually configure IP settings is selected. |
Copy from Module B | Populates the IP Settings Configuration from Module B on the basis of the connection type and the IP settings configuration mode of Module A. Copy from Module B is only available while in Scanner mode and Manually configure IP settings is selected. |
Provide Feedback