Physical device does not match project file
The physical device does not match the device that is configured in the project file.
Make sure that the physical device matches the device that is configured in the project file and select
Retry communication
to establish communication with the device.Provide Feedback