Device definition parameters
Device definition
includes these parameters.
TIP:
The parameters and values are based on the device being configured. The parameters and values that do not apply to the device are hidden.
Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Change type | Select to change the device type and revision. |
Name | Enter an IEC 61131 compliant device name. If an invalid character is entered in this field, or if the name exceeds 40 characters, the software ignores the character. |
Description | Enter the description of the device. Tip : The description must be within 128 characters. If the description exceeds the maximum length, the software ignores any extra characters. |
Ethernet Address | Specifies the IP configuration for the device. Possible options include:
|
Ethernet Address Module 1 Ethernet Address Module 2 | Specifies the ethernet address for Module 1 and Module 2. These two parameters are only available when the criteria are met:
|
Slot | Specify the slot number where the device resides. Only slots between 1 and the maximum number of I/O devices are valid depending on the platform. When the device is created, the slot number defaults to the first available slot position. When the controller is changed to one supporting a smaller maximum I/O count, the current slot value may no longer be valid. |
Module A/B slot | Specifies the slot number where Module A or Module B resides. |
Series | Species the series of the device. |
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Connection | Specifies the rack connection to communicate with the I/O device in the remote chassis. Valid values include:
Tip : The available values depend on the device type. Rack Optimization and Listen Only - Rack Optimization are only available when the device is an adapter in the topology. |
Rack connection | Specifies the connection to communicate with the I/O devices in the remote chassis. Valid values include:
Tip : Data - Rack Optimized and Listen Only - Data - Rack Optimized are only available when the device is an adapter in the topology. |
Time sync connection | Specifies the connection for the device that support Precision Time Protocol (PTP) synchronization. Valid values include:
|
Time sync and motion connection | Specifies the connection for the device that support Precision Time Protocol (PTP) synchronization. Valid values include:
|
Concurrent communication | Valid values include:
|
Redundant | Indicates whether the device supports controller redundancy. Valid values include:
|
Status connection | Specifies the status connect for the device. Valid values include:
|
Network mode | Possible options include:
|
Chassis size | Sets the chassis size of the rack that contains the adapter bridge device. Only the valid chassis sizes are displayed. The chassis size cannot be set to a size that is less than the last device in the chassis. Tip : Chassis size is only available when the device is an adapter in the topology. |
Provide Feedback