Device definition
Use
Device Definition
to:- View the device type.
- Configure device-specific settings.TIP:The parameters are based on the device being configured. The parameters that do not apply to the device are hidden.
Provide Feedback