Connection and Data Format
Change the device definition at any time without deleting the existing device and creating a new device. The profile attempts to display all configuration data for the new settings. Sets to a default value any configuration data that cannot be shown. After applying the new settings, these settings become the base configuration and all previous data format configurations are lost.
A System Issue exists with the Combo device that you must resolve before Input is implemented. The Input connection must generate a partial Configuration data type to just configure inputs.
Parameter | Description |
|---|---|
Input | Generates the input and configuration data types and tags. If the connection is established, the connection owns the configuration data and shares the input data. |
Output | Generates the input, output, and configuration data types and tags. If the connection is established, the connection owns the configuration and output data and shares the input data. |
Provide Feedback