Confirm the changes to the definition of a device
Use the settings in
Apply changes
to confirm any changes that are being made to the device’s definition.To confirm the changes to the definition of a device
- InApply changes, selectYesto update the appropriate values.Data is recovered from the previous definition's settings or set to their default values, as appropriate. Configurations are updated, as required for the new device definition.TIP:The changes are not applied to the software project and only exist within the scope of the profile. To make the changes to the project, selectOK.
Provide Feedback