Retrieve and display latest data from the device
On the tab for the device, the views that are associated with Add-On Profiles do not automatically refresh with the latest data from the device. A
Refresh
link appears that allows you to manually refresh the data. Use the link to retrieve and display the latest data from the device.
TIP:
If you made changes to the data on the tab for the device, write the data to the device prior to selecting
Refresh
. Any changes not written to the device are lost if you select Refresh
prior to selecting Set
.To retrieve and display latest data from the device
- On the tab for the device, in the view in which you are viewing information, selectRefresh.The latest data from the device is retrieved and displayed.
Provide Feedback