Overview view parameters (Ethernet Bridge)

The
Overview
view includes these parameters.
TIP:
Some parameters in the
Overview
view are not available for all device types. To change the configuration, go to the
Device definition
dialog box.
Parameter
Description
Device type
Displays the device catalog number and type.
Vendor
Displays the device manufacturer information.
Description
Displays the device description.
Series
Displays the device series.
Revision
Displays the device major and minor revisions.
Electronic keying
Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
Valid values include:
  • Exact Match
  • Compatible Module
  • Disable Keying
For detailed information on Electronic keying, see Electronic Keying in
Logix5000
Control Systems Application Technique
, publication LOGIX-AT001.
Connection
Displays the Connection Type and the Communication Format.
Rack Connection
Displays the connection to communicate with the I/O devices in the remote chassis. Valid values include:
  • None
    - Direct connection from the controller to the device.
  • Data
    - Data is limited to the basic status and input data in order to optimize the number of connections via a Rack Connection.
  • Listen Only - Data
    - An I/O connection where another controller owns/provides the configuration data for the device. A controller using a listen only connection does not write configuration. It can only establish a connection for the device when the owner controller is actively controlling.
Time Sync Connection
Specifies the connection for the device that supports Precision Time Protocol (PTP) synchronization. Valid values include:
  • None
    - Disables motion and time synchronization in the device.
  • Time Sync and Motion
    - Enables motion and time synchronization in the device.
Time Sync and Motion Connection
Specifies the connection for the device that support Precision Time Protocol (PTP) synchronization. Valid values include:
  • No
    - Disables motion and time synchronization in the device.
  • Yes
    - Enables motion and time synchronization in the device.
Concurrent Connection
Valid values include:
  • No
    - Standard Forward Open.
  • Yes
    - Concurrent Forward Open.
Redundant
Indicates whether the device supports controller redundancy.
Status Connection
Displays the status connect for the device. Valid values include:
  • No
    - No status connection from controller to the device.
  • Status
    - An input connection to the device, used to send bridge/adapter status to the controller.
Network Mode
Valid values include:
  • Device Level Ring (DLR)
  • Parallel Redundancy Protocol
    (PRP)
Chassis size
Displays the chassis size of the rack that contains the bridge device.
Device definition
Opens
Device definition
to change the revision, electronic keying, and other device specific values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal