Display view parameters

Use the
Display
view to configure the display object. The parameters are available when the software is online, and there is no communication error in the device profile.
For duplex devices, you can view the configurations for Module A and Module B. The displayed values become blank in these conditions:
  • There is a device type mismatch.
  • A timeout occurs while getting the identity from a device.
The
Display
view includes these parameters:
Parameter
Description
Enable LCD display of non-system messages
Select to allow all non-system messages to appear.
This parameter is disabled if the device is in explicit protection mode.
Display network configuration messages
Select to display network configuration messages.
This parameter is available when
Enable LCD display of non-system messages
is selected.
This parameter is disabled if the device is in explicit protection mode.
Display uncategorized messages
Select to display uncategorized messages. Uncategorized messages include all messages not covered in the network configuration and non-system messages.
This parameter is available when
Enable LCD display of non-system messages
is selected.
This parameter is disabled if the device is in protection mode.
Refresh
Retrieves and displays the latest values from the device.
Set
Writes pending edits to the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal