Note: Omori India is a Gold OEM Partner of Rockwell Automation.
Omori India Pvt Ltd is a leading manufacturer of high-speed flow wrap machines and automatic feeding and product handling systems for food and non-food applications with over 3100 installations across Asia, the Middle East, and Africa. Their machines are used for wrapping all kinds of biscuits and cookies, chocolate bars, cereal bars, nutraceutical / snack bars, noodle cakes and such other food products. Omori goes beyond just the machinery to provide end-to-end line design and support services – from planning through implementation and ongoing support – for the entire packaging process. Our team combines deep experience in engineering and flexible packaging when providing innovative solutions that result in optimized packaging cost per unit, throughput, and quality for our customers.
- Regulatory compliance barrier
- Complexity of 21 CFR requirements
- Market entry constraints
- FactoryTalk® Optix™ SCADA Software
- CompactLogix™
- Kinetix® 5500 Servo Drives EtherNet/IP
- Kinetix® VP Servo Motors
- Regulatory compliance & market expansion
- Enhanced operational efficiency
- Connected enterprise & data-driven decisions
Challenge
Breaking Barriers to Achieve 21 CFR Compliance for Pharma Market Entry
Omori manufactures wrapper machines for the food and beverage and consumer packaged goods customers. The company wanted to expand into wrapping solutions for the pharmaceutical segment. The biggest roadblock to achieving this for Omori was ensuring that the machine complied with the 21 CFR Code of Federal Regulations.
The 21 CFR and its recommendations are critical in today’s pharmaceutical industry. Title 21 of the CFR, or the Code of Federal Regulations, governs food and drugs in the United States under three regulatory bodies: the FDA (Food and Drug Administration), DEA (Drug Enforcement Administration), and ONDCP (Office of National Drug Control Policy). It consists of three chapters, each specializing in codes for these organizations. Most OEMs must comply with 21 CFR Part 11.
Part 11 applies to drug makers, medical device manufacturers, biotech companies, biologics developers, CROs, and other FDA-regulated industries, with some specific exceptions. It requires implementing controls such as system validations, audit trails, electronic signatures, and documentation for software and systems involved in processing electronic data that FDA require them to maintain. A predicate rule is any requirement set forth in the Federal Food, Drug, and Cosmetic Act, the Public Health Service Act, or any FDA regulation other than Part 11.
Solution
Smart, Compliant, and Connected Blister Packaging Solution
Omori collaborated with Rockwell Automation to develop a new machine for the pharmaceutical segment – blister packaging solutions.
This machine runs on FactoryTalk® Optix™ SCADA software, complying with 21 CFR Part 11 through controls that include audits, system validations, audit trails, electronic signatures, and documentation required for compliance purposes.
CompactLogix™ controllers provide higher performance, increased capacity, improved productivity, and enhanced security to meet the growing demands of smart machines and manufacturing equipment. These controllers use a common, easy-to-use development environment. Tighter integration between the programming software, controller, and I/O modules reduces development time and cost during commissioning and normal operation. This commonality enables cost-effective integration of a machine or safety application into a plant-wide control system because it consolidates capabilities into one controller.
Kinetix® 5500 Servo Drives EtherNet/IP connect to and operate with CompactLogix™ controllers, supporting Integrated Motion on EtherNet/IP. With its innovative, compact design, the Kinetix® 5500 drive helps minimize machine footprint and simplifies system wiring.
Kinetix® VP Servo Motors provide smooth, integrated motion control over EtherNet/IP networks and are optimized to run alongside the Kinetix® 5500 and 5700 servo drives. Kinetix® VPL low-inertia servo motors deliver higher dynamic performance.
The multi-axis machine is now smarter, as seamless data transfer is possible via Ethernet communication. Based on the type of product, the end user can select a recipe from the human-machine interface, and the system will make automatic offset adjustments. The absolute position of the servos can be retained in case of a power failure.
End users benefit from higher accuracy and lower maintenance with a reduced mechanical system, and scalability is achievable through axis addition or deletion. Integration with upstream systems is now easier than ever.
Result
Delivering Compliance, Connectivity, and Operational Excellence
The scalable machine developed by Omori using Rockwell Automation’s solutions can now serve pharmaceutical industry end users with multiple packaging solutions.
Remote operation and monitoring of the machine are now possible, as the multi-discipline architecture can be accessed remotely for troubleshooting or modification, eliminating the need for physical site visits.
EtherNet/IP connectivity enables The Connected Enterprise™, converging plant-level and enterprise networks while securely connecting people, processes, and technologies. Connected smart devices provide new visibility into processes, and data and analytics from these machines enable better and faster decision-making. Seamless connectivity also fosters improved collaboration.
Published February 25, 2026
You may also be interested in