Synchronization and Switchover for Communication Module Series Replacement

If electronic keying is not set to Exact Match, follow these steps to replace communication modules with a new series.
  1. Make sure the existing modules and the new series modules use the same IP address, network mask, and gateway address.
  2. Make sure that the RMCT version is compatible with your redundancy firmware.
  3. Make sure that the redundancy module firmware is at the firmware revision for the specified bundle.
  4. Go online with the primary controller.
  5. For each module, verify that the Electronic Keying is set to Compatible Module or Disable Keying.
    Electronic Keying set to Compatible Module
  6. Access the RMCT for a redundancy module in either chassis.
  7. On the Configuration tab, set Auto-synchronization to Never.
    Auto-Synchronization set to Never
  8. Select Apply.
  9. On the Synchronization tab, select Disqualify Secondary.
    Disqualify Secondary command
  10. Make a note of the port configuration of the secondary communication module:
    • IP address
    • Network mask
    • Gateway address
  11. Disconnect the Ethernet cables from the secondary communication module.
  12. Turn off power to the secondary chassis.
  13. Remove the communication module from the secondary chassis.
  14. Set the switches on the new series communication module to 888, insert the module in the secondary chassis, and apply power to the chassis.
    1. After the reset is complete, turn power off to the secondary chassis and remove the module from the secondary chassis.
    2. Set the switches to the same settings as on the module that was removed.
    3. Reinsert the module into the secondary chassis, reattach the cable, and apply power to the secondary chassis.
    4. To support bridging across the backplane or USB port, configure the port configuration of the secondary module to match the port configuration of the primary module.
  15. Update the firmware of the new communication module.
  16. After the update completes, connect the Ethernet cable to the secondary communication module and wait for communication to resume on the network.
  17. Repeat steps 10…15.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal