Output Operation

For output modules, sourcing safety outputs can be configured as point operation type single or dual. The selected type configures the safety module to treat the outputs individually or as a pair:
  • A single configuration allows the outputs to turn on and off individually and to fault independently.
  • A dual configuration verifies that safety task logic operates both outputs as a pair. If one output has a module fault, the other output goes to the safe state.
Output Point Operation Types
Output Point Operation Types
Bipolar outputs have no configuration for point operation type and must operate as a sinking sourcing pair.
IMPORTANT: The point operation type affects the PFH safety rating of the module. The PFH is theĀ average frequency of a dangerous failure per hour.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal