Controller and Software Compatibility
Controller and programming software compatibility requirements apply when you use
PointMax I/O modules. A module type and how it is used affect which requirements
apply.
You must use Studio 5000 Logix Designer application version 36 or later. For more
information, see the Product Compatibility and Download Center at rok.auto/pcdc.
If you use GuardLogix® controllers and need to use up to chassis
slot 32, you must use Studio 5000 Logix Designer application version 37 or later.
Provide Feedback