Axisxx – Homing View

Use Axisxx – Homing to view or configure the homing parameters of the specific axis.
Axisxx – Homing View Example
The Axisxx – Homing view includes these parameters:
Parameter
Description
Home Speed
Specifies the speed to use during a Home operation until the home limit switch is detected. You can set this parameter to a high value to reduce the time it takes to perform the Home command.
Valid values are greater than 0.0 and less than or equal to C:MaxSpeed.
The value is in Engineering Units per second.
Home Final Speed
Specifies the final speed to use after the home limit switch is detected. You can set this parameter to a low value to achieve better home position accuracy.
Valid values are greater than 0.0 and less than or equal to C:MaxSpeed.
The value is in Engineering Units per second.
Home Acceleration
Specifies the speed's rate of change when performing the Home command.
The value is in Engineering Units per second
2
.
Home Timeout
Specifies the maximum time that the axis is allowed to find the home position.
When the time elapses, the axis performs a smooth stop and position remains invalid.
Valid values are 1.0…600.0 seconds
Home Position
Displays the position value to set as the current position when a Home or Set Home Position command completes.
The value is in Engineering Units.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal