Short Circuit Detection
IMPORTANT:
This feature is available only in Voltage (V)
mode.
Short Circuit Detection helps prevent damage that can result from a mis-wiring or driving
a current from the channel greater than the maximum current level the channel can
handle.
When a short circuit condition is detected, the following occurs:
- The output turns off.
- TheI.Chxx.ShortCircuittag is set to 1.
For more information on the maximum current that you can apply to an output, see the
PointMax I/O System Specifications Technical Data, publication 5034-TD001.
Provide Feedback