Field Power (SA Power) Loss Detection

The Field Power Loss Detection feature monitors for the loss of field-side power on the SA power bus. It has a corresponding channel level tag that can be examined in the user program if a fault occurs. When field power to the module is lost, the channel level field power loss bit and fault bit are set for all channels and sent to the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal