Time Synchronization View
The Time Synchronization view is read-only and displays the CIP Sync
status information about the module when the project is online. The Time Synchronization
category displays the following information:
- CIP Sync time synchronization status
- UTC system time
- Grandmaster Clock information
- Grandmaster Clock description
- Local Clock information
Time Sync View Example

Grandmaster Clock Description
The Grandmaster clock description dialog provides detailed
information about the grandmaster clock. To view the Grandmaster clock description, select
Description in the Time Sync view.
Grandmaster Clock Description Example

Provide Feedback