Device Configuration

This section describes how to add and monitor HART devices that are connected to your analog HART input or output module in a Studio 5000 Logix Designer application project.
  • Some HART device profiles are pre-loaded in the Studio 5000 Logix Designer application and are recognized when you connect them to HART enabled channels.
  • Some HART devices need Electronic Device Description (EDD) information updates before you can use them.
  • Some HART devices are not recognized and need generic profiles to connect to the channels.
TIP:
In an output module, the power to the field device is provided by the channel. If the channel is not energized, the HART device is not powered on.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal