Troubleshoot Wiring Issues
The possible faults that can occur due to incorrect usage or when wiring IO-Link master
module are listed here.
System/Function | Fault | Description | Recommended Action |
|---|---|---|---|
I/O Port
| |||
Configurable I/O | Configured as output but wired as input. Two operating outputs
are joined. | Module operates. However, a fault is reported if excess current
is drawn from the module due to the difference in potentials and the
affected channel switches off. | Complete the following steps:
|
Provide Feedback