Short Circuit Detection
Short circuit detection helps prevent damage that can result from driving a current from
the channel greater than the maximum current level that the channel can handle.
Ports | Short Circuit Conditions with Detection | Description |
|---|---|---|
0, 1, 2, 3 | SSV Power Short Circuit | Short between terminals V+ and COM |
Odd Channel Output Short Circuit | Short between terminals I/Q and COM | |
Even Channel Output Short Circuit | Short between terminals C/Q and COM |
When a short circuit condition is detected, the following occurs:
- The channel limits the output current and monitors for the short circuit condition to be removed.
- The I/O status indicator for the channel flashes red.
- TheI.IOLinkxx.FaultorI.Ptxx.Faulttag is set to 1.
Check the channel diagnostic or retrieve the information from the diagnostic assembly to
verify that the short circuit condition is present.
When the short circuit condition is removed, the following occurs:
- The channel restarts in its commanded state.
- The I/O status indicator for the channel turns back to steady yellow.
- TheI.IOLinkxx.FaultorI.Ptxx.Faulttag is reset to 0.
Check the channel diagnostic or retrieve the information from the diagnostic assembly to
verify that the short circuit condition is removed.
To check the channel diagnostics, see Channels View.
For more information on how to retrieve diagnostic assemblies, see Diagnostic Assembly.
For more information on using module tags, see 5034-IOL4 and 5034-IOL4XT Details .
Provide Feedback