Input Timestamping

Timestamping registers a time reference to a change in input data. CIP Sync is used for timestamping when the channel is configured as “Digital Input, Timestamp” or “Digital Input, Timestamp, Fallback”.
The IO-Link master module offers submillisecond timestamping on a per channel basis.

Pulse Latching

Pulse Latching is supported via the Timestamping feature and Timestamp Latching. You can use Pulse Latching to detect or latch short-duration pulses.
To use Pulse Latching, you must configure the channel as “Digital Input, Timestamp” or “Digital, Input, Timestamp, Fallback”. See Device Definition - Channel Assignments View.
Location in Studio 5000 Logix Designer Application Project
Action
Module Properties → Overview → Device Definition → Channel Assignments
Check the input transition type where you must latch short-duration pulses.
For example, for short-duration pulses that are latched for Off to On transitions, select Off → On input transition.
Module tags
One or both of these actions.
  • Change the
    C.Ptxx.CaptureOffOnEn
    tag to 1.
  • Change the
    C.Ptxx.CaptureOnOffEn
    tag to 1.
When the module detects a short-duration pulse at an input point, the changes that are described in this table occur.
Input Transition Type Where Pulse Is Captured
Change in Studio 5000 Logix Designer Application Project
Off to On
  • The
    I.Ptxx.TimestampOffOnNumber
    tag increments.
  • The timestamp is recorded in the
    I.Ptxx.TimestampOffOn
    tag.
On to Off
  • The
    I.Ptxx.TimestampOnOffNumber
    tag increments.
  • The time stamp is recorded in the
    I.Ptxx.TimestampOnOff
    tag.
When subsequent short-duration pulses are detected at the same input point, the Latching configuration dictates what changes, if any, occur in the Studio 5000 Logix Designer application project.
Latching Configuration
Input Transition Type Where Pulse Is Captured
Change in Studio 5000 Logix Designer Application Project
Disabled (default)
These conditions disable Timestamp Latching.
  • The Enable Timestamp Latching checkbox on the PTxx page is cleared.
  • The
    C.Ptxx.TimestampLatchEn
    tag = 0
Off to On
The
I.Ptxx.TimestampOffOnNumber
tag increments.
The new time stamp is recorded in the
I.Ptxx.TimestampOffOn
tag, which overwrites the previous time stamp.
On to Off
The
I.Ptxx.TimestampOnOffNumber
tag increments.
The new time stamp is recorded in the
I.Ptxx.TimestampOnOff
tag, which overwrites the previous time stamp.
Enabled
These conditions enable Timestamp Latching.
  • The Enable Timestamp Latching checkbox on the PTxx page is selected.
  • The
    C.Ptxx.TimestampLatchEn
    tag = 1
Off to On
The
I.Ptxx.TimestampOffOnNumber
and
I.Ptxx.TimestampOffOn
tags remain latched until the last captured pulse is acknowledged. In other words, the tag values remain the same until the last captured pulse is acknowledged.
On to Off
The
I.Ptxx.TimestampOnOffNumber
and
I.Ptxx.TimestampOnOff
tags remain latched until the last captured pulse is acknowledged. In other words, the tag values remain the same until the last captured pulse is acknowledged.
To acknowledge the last captured pulse, set the output tag of the last input pulse as follows:
  • Off to On transition - Set the
    O.Ptxx.TimestampOffOnNumberAck
    tag =
    I.Ptxx.TimestampOffOnNumber
    tag.
  • On to Off transition - Set the
    O.Ptxx.TimestampOnOffNumberAck
    tag =
    I.Ptxx.TimestampOnOffNumber
    tag.
Once a pulse latch is acknowledged for an input point, the next pulse at that point increments the corresponding
I.Ptxx.TimestampOffOnNumber
and records the time stamp in
I.Ptxx.TimestampOffOn
.
You can change tag values in program logic while normal module operation continues or through the Studio 5000 Logix Designer application tag editor.

Chatter Detection

Chatter Detection is a feature that is directly related to Timestamping. You use the feature to detect when a device that is connected to the module input causes chatter.
Chatter occurs when the device causes the inputs to transition falsely many times in a relatively short period. As a result, the module timestamps invalid input transitions.
You can configure the following:
  • Chatter Count
    – Determines the number of acceptable input transitions that can occur in a given time period before considering the input to be chatter.
    Valid chatter count values range from 2…127.
  • Chatter Time
    – Determines the amount of time within which the number of input transitions are counted.
    Valid chatter time values range from 1…10000 ms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal