Update Device Firmware
If your Rockwell Automation IO-Link device has firmware
revisions that are available in PCDC, you can use ControlFLASH Plus®
software version 6.00 or later to update the firmware of the device that is attached to
your IO-Link master module.
During the firmware update process, you cannot change the operating mode of the
channel.
For more information on how to use the ControlFLASH Plus software, see the ControlFLASH
Plus Quick Start Guide, publication CFP-QS001.
Provide Feedback