IO-Link Events
The IO-Link master module supports both IO-Link port-level and
IO-Link device-level reporting of IO-Link events.
Port/Device | With Timestamp | Maximum Number of Events |
|---|---|---|
IO-Link Port | Yes | 40 per port |
IO-Link Device | Yes | 40 per device |
No | 124 per device |
Timestamps for port-level IO-Link events are always enabled. To view the port-level
IO-Link event log, see Channels View.
To enable timestamps for device-level IO-Link events and view the device-level IO-Link
event log, see Event Log View.
For more information on the IO-Link Event Log, see IO-Link Event Log.
Provide Feedback