IO-Link Bus
Every IO-Link device is added as a CIP node on the IO-Link bus that is
associated with the IO-Link master module.

You can use the IO-Link bus in the I/O Configuration tree to:
- Add or remove an IO-Link device.
- See the warning or inhibit status icon of an attached IO-Link device.
- Open the properties for the IO-Link device.
Provide Feedback