Device Configuration

You can use the Configuration view to change configurations for the IO-Link device. The parameters that are shown in the Configuration view are based on the device IODD.
The Configuration view shows the parameter values that are saved in the Studio 5000 Logix Designer application project. The values that are shown in the Configuration view do not reflect the actual values of the parameters in the device.
All configuration parameters are stored in the project, but the device may have the set of configuration parameters that are shown in the Configuration view change based on the conditional parameters that are defined in the device IODD.
One exception is the parameter that is used to select which set of process data to use. When the device is on an IO-Link channel (excluding Fallback channels), this parameter is not shown in the Configuration view because it affects the input/output data tag definitions and can only be changed through the connection type selection in the Module Definition dialog in offline mode.
In offline mode, you can use the Configuration view to change the device configuration and save the values to the project.
In online mode, when you apply the configuration, the configuration is saved to the project and set to the device.
If a parameter is not listed under any menu in the IO-Link device IODD, the parameter is ignored and not shown on any view in the IO-Link device Module Properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal