Automatic Device Configuration

Automatic Device Configuration (ADC) provides an automated download of an IO-Link device configuration from the controller to the IO-Link device when the controller opens the device connection.
You can use ADC to help simplify device replacement, or to clone your device configuration across multiple systems with the same physical setup easily.
Whenever a connection is established, the IO-Link device configuration that is saved in the controller is set to the device. This device configuration is accessible from the Module Properties window in the Studio 5000 Logix Designer application or device configuration tag.

Configuration Tags

When you add an IO-Link device with ADC enabled, configuration tags are created based on the configuration parameters that are available in the device IODD.
The benefit of having configuration tags is that the ladder program can use the configuration tags to change the device configuration with programming logic.
The configuration tags can be used before or when the connection is open:
  • Before the connection is open, the ladder program inhibits the device, changes the configuration tag, and uninhibits the device.
  • During an open connection, the ladder program changes the configuration tag and issues a reconfiguration instruction. For more information, see Configure IO-Link Device through Configuration Tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal