Register Embedded IODD Files
IMPORTANT:
This section applies only to IO-Link devices from
Rockwell Automation that have an embedded IODD file.
To use FactoryTalk Linx software version 6.40 or later to upload and register the embedded
IODD file in IO-Link devices, complete these steps.
- In the FactoryTalk Linx Network Browser, select a device in the communication tree.
- Right-click the device and select EDS / Device Description Upload.
- If the target device has registered a device description file, the following warning message shows:“An EDS / Device Description is already registered for this device. Are you sure you still want to upload and register this EDS / Device Description file?”Select OK to continue and replace the existing device description file, or select Cancel to stop the upload process and retain the existing device description file.
Provide Feedback