Adjust Device Configuration After Replacement

After you have successfully replaced an IO-Link device, you can adjust the device configuration with one of the following methods.
  • Use the Configuration view in the IO-Link device Module Properties.
  • If ADC is enabled for the IO-Link device, you can change the configuration tag values and apply the reconfigure instruction from the ladder program.
  • Send connected explicit messages from the controller ladder program to change the device configuration and use the
    ParamDownloadStore
    command (index 02, value 0x05) to trigger a back up to the IO-Link master module. For more information, see Data Storage.
  • Use the physical controls on the IO-Link device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal