Add a New Module

TIP: You can use the new module method when the project is offline or online.
To use the New Module method, complete these steps.
  1. In the I/O Configuration tree, right-click the IO-Link bus and select New Module.
    The Select Module Type dialog appears.
  2. Select the device and select Create.
    To narrow down the list of devices, use the filters or search with keywords.
    The New Module window appears and shows the General view.
  3. Enter a Name for the device.
    If you want to configure the other settings during this step, see IO-Link Device Configuration for more information.
  4. Select OK to save the configuration.
    If you are in online mode, a prompt appears to request to inhibit the device. We recommend inhibiting the device if the device is not fully configured or not ready to be put into operation currently.
  5. Repeat Step 2...Step 4 to add another device, or close the Select Module Type dialog. If you selected the Close on Create checkbox in Step 2, you must start from Step 1 to add another device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal