To use a MAOC instruction with schedule outputs, complete the following steps:
IMPORTANT:
  • Before you complete the steps, confirm that Time Synchronization is enabled in the controller and, if applicable, the Ethernet module, to use scheduled outputs.
  • You must verify in your logic that the grandmaster clock ID in both the controller and I/O module is identical. For more information, see Grandmaster Clock Verification.
  1. If necessary, add an output module to your Studio 5000 Logix Designer application project.
  2. From the Overview in the Module Properties dialog, select Device definition to access the Device Definition parameters.
  3. For 5034-OB16 and 5034-OB8 modules:
    In the Device Definition dialog, choose Scheduled Data for the Output Data.
    For 5034-UB8 and 5034-UB8F modules:
    In the Device Definition dialog, choose Yes for the MAOC Compatible Data.
  4. Select OK to close the Device Definition dialog.
  5. Add an MAOC instruction to your logic.
  6. In the MAOC instruction, use the module output tag in the Output operand, for example, Adapter:1:O for the output module.
    The tag value displays as ??. This value is correct.
For more information on how to use an MAOC instruction in general, see the following:
  • Logix 5000 Controllers Motion Instructions Reference Manual, publication MOTION-RM002
  • Position-based Output Control with the MAOC Instruction Application Technique, publication 1756-AT017
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal